Technical FAQs

Ask a Question

What is the part number for a green pilot light lens for XACA Pendant Station?

Issue: 
What is the part number for a green pilot light lens for XACA Pendant Station ?

Product Line: 
Pendant Station 

Environment:
NEMA 1,3R ,4 , 12
IP55 IP65

Cause:
Catalog does not show replacement parts  

Resolution:
ZA2BV03 and the ZA2 operators are used on the XACA Pendant Station
Was this helpful?
What can we do to improve the information ?