Technical FAQs

Ask a Question

During the installation of Vijeo Historian V4.40, SQL is not installed and it shows the error message " Error in extracting SQL Server 2008 ".

As per the given error details this seems to be issue with either of the mentioned points

1. Your system security like "User Account Control" (UAC) should be set to "never notify" and other firewall / antivirus should be disabled when you start your installation setup. 
2. There is not enough memory in your hard drive for SQL installation. So kindly check that your system space is enough. 
3. The SQL Server installation is not properly extracted so this may occur if you have an ISO image and while converting it there is some file corrupted. So for you need to
properly unzip Vijeo Historian files properly.  Still if you were facing this error then try to install SQL Server setup separately which is available in the following path in the
installation file "HistorianV4.4\Historian\Extras\1033\SQL Server" 
Was this helpful?
What can we do to improve the information ?