Technical FAQs

Ask a Question

We try to installed Vijeo Historian software from DVD and Local HDD but got the below error message : "There was a problem installing SQL Server 2008R2. Do you want to continue installing Vijeo Historian"  What could be the reason for this error.

This error may occurs due to SQL password which you set during Vijeo Historian installation.  This SQL Server SA User Account dialog
requires you to select a password for the administrator account that will be created for the new instance of SQL Server. The password needs
to be at least five characters, and cannot be one of the following:  >>password  >>admin  >>administrator  >>sa  >>sysadmin  If the computer
you are installing on is running Microsoft Windows 2003 and joined to a domain, the password should also meet the strong password complexity
requirements of your domain.  Keep a record of this password, as you may need it at a later date to manage your SQL Server databases. 
Was this helpful?
What can we do to improve the information ?