Technical FAQs

Ask a Question

We have upgraded our project backup from VJC version 6.10 to Version 7.30 . Now when we starts the Vijeo Citect runtime, we got the error message "Cannot Create Task IOServer".

If there is a "|" (vertical bar ) or any special character sign is added by mistake after a IO Device name during the project upgrade time which is causing runtime to crash .
After removing this sign the problem will resolves.
Was this helpful?
What can we do to improve the information ?