Technical FAQs

Ask a Question

What is trigger value for UPA [Undervoltage warning ] in Altivar 61 / 71 / 32 range of drives .

For ATV61 / ATV71 / ATV32 range of drives, The UPA [Under voltage warning] is linked to the “undervoltage management” function.
If the “undervoltage prevention” (“StP”) parameter is not set to “No” then you have access to the “prevention level” (“UPL”) parameter.
This parameter (“UPL”) is the trigger value. The voltage level of “UPL” is defined by the drive voltage rating and the “main voltage” (“UrES”) value. 
 
Was this helpful?
What can we do to improve the information ?