Technical FAQs

Ask a Question

What is the nominal output current value at 415 volts for ATV71**N4  range of drives

For ATV71**N4 range of drives, nominal output current at 415 volts can be derived using formula



Within formula , i3 is the nominal current at 415V ,i1 is continuous output current value at 380 volts and i2 is continuous
output current value at 460 volts as described in catalog.

Was this helpful?
What can we do to improve the information ?