Technical FAQs

Ask a Question

What is  the maximum load resistance for pressure transmitter of XMLE range with 4-20 mA output.

For Electronic pressure sensors of range XMLE maximum load resistance can be calculated using common formula as below,
R load max = U supply - U supply min / 0.02A
 
For XMLE range of pressure sensors have supply range = 11..33 VDC and Sensors with
digital display have supply range = 19..33 VDC
 
Rload Max for sensors, substituting U supply = 33 VDC and Usupply min = 11 VDC then
Rload Max = (33-11) / 0.02 = 1100 Ohms.

Rload Max for sensors with digital display, substituting U supply = 33 VDC and Usupply min = 19 VDC then
Rload Max = (33-19) / 0.02 = 700 Ohms.
 
Was this helpful?
What can we do to improve the information ?