Technical FAQs

Ask a Question

Can the LUCA12BL be controlled with a PLC?

Issue:
The LUCA12BL is to be controlled directly with the output of a PLC.

Product Line:
Tesys U line

Environment:
LUB32+LUCA12BL

Cause:
PLC doing remote control of the motor starter.

Resolution:
Yes, if the output of the PLC is 24 V DC and can handle an inrush of 220mA . A reversing module will add 120mA to the inrush when it has to change the direction of the motor.
Was this helpful?
What can we do to improve the information ?