Technical FAQs

Ask a Question

How many Analog Inputs available in Altivar 312 drive.

There are 3 analog inputs:
2 voltage inputs:
0-10 V (AI1)
± 1 0 V (AI2)
 
1 current input:
X-Y mA (AI3), where X is configurable between 0 and 20 mA, and Y is configurable between 4 and 20 mA
Was this helpful?
What can we do to improve the information ?