Technical FAQs

Ask a Question

What is the max distance for the Wireless (Harmony) pushbuttons without a relay antenna

 The maximum distance is 100m without obstructions, this is reduced to 25m if the receiver is enclosed in a metal enclosure.
Was this helpful?
What can we do to improve the information ?