Technical FAQs

Ask a Question

What is the part code for an illuminated latching push buttons to go into a XACA08 pendant?

There are no illuminated latching push buttons in our pendant range.
The only latching options are either a mushroom (ZA2BS834 30mm or ZA2BS844 40mm) or selector switch (ZA2BD2 2 position), neither of which are illuminated.
Was this helpful?
What can we do to improve the information ?