Technical FAQs

Ask a Question

What is the part code for a 16A Relay Module?

 The PDL600RM is rated 16A resistive (6A inductive) and has a NO & NC contact. It is a 600 series module so can be mounted in a grid plate, but doesn't have to be as there is no built in indication as to the state of the contacts.
Was this helpful?
What can we do to improve the information ?