Technical FAQs

Ask a Question

What code is a multi voltage inductive proximity with sensing distance 0-8 mm?

XS8E1A1MAL2 = rectangular plastic, prewired, N/O 26 x 26 x 13mm with 0-8 mm range
XS630B1MAL2 = cylindrical metal, prewired, N/O 30 x 60mm with 0-12 mm range
XS4P30MA230 = cylindrical plastic, prewired, N/O 30 x 60mm with 0-12 mm range
Data sheets attached, other options may also be suitable depending on requirements.
Was this helpful?
What can we do to improve the information ?