Technical FAQs

Ask a Question

How to set up the ATV61 HMI keypad to display more than one parameter?

Issue:
Keypad display screen shows only one parameter
 
Product line:

Altivar 61 and 71

Environment:

All models, all serial numbers:
 
Cause:
One parameter is the default.
 
Resolution:
From the main menu go to menu 6 [Monitoring Config] then enter
Select 6.2 [MONITOR SCREEN TYPE].  
If "Digital value type" is "Digital" only two parameters can be selected.
If "Digital value type" is "Bar graph" only two parameters can be selected.
If "Digital value type" is "List" then five parameters can be selected.
Go to "PARAMETER SELECTION".  Select the check box beside the parameters you want to display.
Was this helpful?
What can we do to improve the information ?