Technical FAQs

Ask a Question

What are options for communicating via ModBus ethernet to the ATS48 ?

Issue:
What are options for communicating via  ModBus ethernet to the ATS48 ?

Product Line:
Altistart  ATS48

Environment:
All 

Cause:
Communications Options

Resolutions:
The softstart has a built-in Modbus port. 
A Modbus to Ethernet Gateway such as the TSXETG100 is also an available option.
Was this helpful?
What can we do to improve the information ?