Technical FAQs

Ask a Question

Can you use two keypads on the ATV61 or ATV71 drives at the same time with a splitter or T adaptor?

Issue:
Can you use two keypads on the ATV61 or ATV71 drives at the same time with a splitter or T adaptor?

Product line:
Altivar ATV61 and ATV71

Environment:
All models, all serial numbers

Cause:
2 keypads on one Drive

Resolution:
There is no way to connect two keypads on one drive at the same time. If you connect two keypads at the
same time you will get a error message on the 2nd keypad that was attached.   
Was this helpful?
What can we do to improve the information ?