Technical FAQs

Ask a Question

What are the priority level of alarms can be configured in PM820

 Each alarm has a priority level. Use the priorities to distinguish between events that require immediate action and those that do not require action.
•    High priority—if a high priority alarm occurs, the display informs you in two ways: the LED backlight on the display flashes until you 
acknowledge the alarm and the alarm icon blinks while the alarm is active.
•    Medium priority—if a medium priority alarm occurs, the alarm icon blinks only while the alarm is active. Once the alarm 
becomes inactive, the alarm icon stops blinking and remains on the display.
•    Low priority—if a low priority alarm occurs, the alarm icon blinks only while the alarm is active. Once the alarm becomes inactive, 
the alarm icon disappears from the display.
•    No priority—if an alarm is setup with no priority, no visible representation will appear on the display. Alarms with no priority 
are not entered in the Alarm Log.
Was this helpful?
What can we do to improve the information ?