Technical FAQs

Ask a Question

What is the allowable load resistance of PM800 series meter optional analogue output PM8M2222 module

As per the specifications of PM800 series meter optional analogue output of PM8M2222 module, allowable load resistance is 600 ohm i.e. Current output range is 20mA into 600 ohm max.
The allowable load resistance specifies either the maximum or minimum load resistance allowed for each output, depending on the output type. If the module is operated with a load exceeding this limit, local overheating may result in component failure or the full output range may not be available. 
Was this helpful?
What can we do to improve the information ?