Technical FAQs

Ask a Question

How to setup PM820 relay output for under voltage alarm

To set up the own alarms for default KY digital output or even after installing an input/output module (PM8M2222) via display. For example, you may need to use 
alarm under voltage to trigger output KY relay of PM820. 
2). Enter the maximum value PU mag=400/OK; pick-up delay PU delay=1/OK; drop-out value DO Mag=390/OK; drop-out delay DO delay=1/OK 
3). Press up button and select "YES" to save the change. 
4). Go to MAINT>SETUP>I/O>D OUT (digital out)-->KY /EDIT/NORM/OK/change EXT. to ALARM 
5). Press to select alarm type: UNDER VAB, to active the alarm, press + until asterisks appearS like: ** AL-XX** 
6). Press up button and select "YES" to save the change. In this way customer is able to customize their own alarm. The contact is as NO mode. 
Was this helpful?
What can we do to improve the information ?