Technical FAQs

Ask a Question

Is there any tripping curve available for Acti9 C60PV-DC range of MCB.

 Please refer the below file for the tripping curves of Acti9 C60PV-DC range of MCB

Acti9 C60PV-DC tripping curve

The Acti9 C60PV-DC offer is a specific offer dedicated to PV applications (based on C60H-DC product but not the same).
C60PV-DC: B curve=> 5.5In +/-20% only for rating 8 to 25A 
          C curve=> 8,5In +/-20% only for rating 1 to 5A
Was this helpful?
What can we do to improve the information ?