Technical FAQs

Ask a Question

Is Shunt coil (MX) and closing coil (XF) of EasyPact CVS 800A continuous rated or not.

The shunt coil (MX) and closing coil (XF) of EasyPact CVS 800A are not continous rated.

However, the shunt coil (MX) and closing coil (XF) of EasyPact CVS 100-630A are continuous rated.
Was this helpful?
What can we do to improve the information ?