Technical FAQs

Ask a Question

What is the rated operational current rating of EasyPact CVS 630A equipped with thermal-magnetic trip unit.

The Easypact CVS 630 has a thermal-magnetic trip unit of TM600D i.e. 600A at 40 degC. 
However at 30 Deg C it can be used upto 625A.

Please refer the below Temperature derating chart.


Was this helpful?
What can we do to improve the information ?