Technical FAQs

Ask a Question

What is the Magic Box in Masterpact NT/NW product range.

Magicbox is an interface for communication between a PC and a Micrologic control unit, via either the test connector on the Micrologic or
the ModBus communication module.
 
Magicbox may serve to send READ, WRITE and other orders using SSU (Schneider Service Utilities, i.e. LDU, RDU, RCU, RSU).
 
The Magicbox case (part No. 47595) includes:
> 1 Magicbox communication interface,
> 1 power cord,
> 1 cable for connection to the PC (RS232),
> 1 cable for connection to the test connector (part No. 33590),
> 1 cable for connection to the ModBus network,
> 1 connector to the terminal block on fixed circuit-breakers,
> 1 connector to the terminal block on drawout circuit-breakers,
> 1 connection guide.
 
Was this helpful?
What can we do to improve the information ?