Technical FAQs

Ask a Question

Why will the analog output not change when the AO1 assignment is set to Torque 4Q?

 The Analog output is fixed at 50% and not changing as the torque in the motor changes (Fixed at 10mA when the Analog output is set to 0-20mA, fixed at 12 mA when the Analog output is set to 4-20mA)
Product Line:
 Altivar 71
 All part numbers all versions
 The motor control type is set to either V/F 2pts or V/F 5pts
The Motor control type must be set to something other than V/F 2pts or V/F 5pts for this function to work.   Once the Motor Control type has been changed the analog output should begin to respond to changes in the motor torque.
Was this helpful?
What can we do to improve the information ?