Technical FAQs

Ask a Question

What RTD's are supported with the Sepam relay

 The Sepam relays support the following three types of RTD's (this only applies to Sepam relays that support the MET148-2 module):
1. PT100 (Platinum 100 ohm)
2. NI100 (Nickel 100 ohm)
3. NI120 (Nickel 120 ohm)
 
Note: The MET148-2 (RTD Module for the Sepam relays) only supports three wire RTD's. This does not mean two wires and a shield.
Was this helpful?
What can we do to improve the information ?