Technical FAQs

Ask a Question

Can we use 140NOC77100 in Quantum Hot standby configuration.

The 140 NOC 771 01 module cannot be placed in a hot-standby rack. For High End Hot standby CPUs only 140 NOC 78x is supported.
140 NOC 77101 does not support Hot Standby system, but support all other Quantum Unity CPU's.
Was this helpful?
What can we do to improve the information ?