Technical FAQs

Ask a Question

What is the maximum number RIO drops are supported on Quantum Ethernet IO system.

 If you use Quantum CPU (140 CPU 6• 1••) (2 MB or less), you can only install a maximum of 31 remote I/O drops. Of those 31 drops, you can only install a
 maximum of sixteen BMX CRA 312 •0 remote I/O drops.
If you use a Quantum CPU (140 CPU 6•2 ••) (4 MB or more), you can only install a maximum of 31 remote I/O drops but with CPU (140 CPU 6•2 ••)  you
can install any combination of BMX CRA 312 •0 or 140 CRA 312 00.
Was this helpful?
What can we do to improve the information ?