Technical FAQs

Ask a Question

When I run project "Example" from Vijeo Citect 7.3 and foundthat the page can be auto resized to fit the full screen resolution (ex: the page in the project is set as 1024x768 and my laptop display is 1366x768. when I click the maximize symbol on the tab, the page become fit to my full screen). Please guide me how to do this in my project.

If you want to show the full screen on your system for the runtime , then you have to set the following INI parameters in your project parameters or set them in your INI file:

[Page]MaintainAspectRatio = 0
[Animator]FullScreen = 1


Was this helpful?
What can we do to improve the information ?