Technical FAQs

Ask a Question

When we installed the Vijeo Historian v4.40 the software installed successfully except the Excel Client.When we tried to manually install the setup, under Clients/Analysis Tools there is only Historian Web Client option is available.

With new Vijeo Historian Ver 4.4 the excel client is replaced with new featured Historian Enquire, which needs to be installed separately from the
installation DVD. In the installation DVD you will find a "Historian Enquire.exe" , you need to run that exe file to install this enquire.

Was this helpful?
What can we do to improve the information ?