Technical FAQs

Ask a Question

When I started the Vijeo Citect runtime, this gives me a error "You are running a restricted MODBUS driver version. The driver is time limited and will go offline after 4 hours".

This error seems to be due to the limited version of the Modbus Driver due to which there is restriction that this driver will only run for 4 hrs .
So to remove this driver error you need to install a full version of the Modbus driver, which you can download from the given below link :

https://schneider-electric.box.com/s/o3w7j0po5ctwiiy70aet

You need to close all the VJC applications & then install this driver and again starts VJC runtime.

Was this helpful?
What can we do to improve the information ?