Technical FAQs

Ask a Question

Are there I/O option cards for the ATS48?

Issue:
Does the ATS48 have an external I/O option card?

Product Line:
ATS48

Environment:
All

Cause
Additional I/O needed.

Resolution: 
There are no external option cards for the ATS48. 

Was this helpful?
What can we do to improve the information ?