Technical FAQs

Ask a Question

Are the replacement coils for the LC1D different from the original coils?

 What are the differences between the coils supplied in the contactors and the replacement coils?
Product Line:
 LC1D contactors 
 LC1D65A and smaller contactors with AC coils
 Different appearance of the coils

The coils supplied in the devices do not have a tape covering, you can see the wire winding. The replacement coils all have tape on the outside of the winding for protection during handling and installation.
Was this helpful?
What can we do to improve the information ?