Technical FAQs

Ask a Question

I am using the vijeo citect ver 7.20. Now I want to use the time scheduler tool with this latest version. How I can use this tool .

This time scheduler utility is now automatically clubbed in Vijeo Citect SCADA with SP3 & there is no seperate license needed for using this tool.  For using this
tool kindly install SP3 on VJC ver 7.20 or later. Then you have to configure Equipment in Citect>> Project Editor >> System >> Equipment and Equipment State.
After that you have to insert a Scheduler ActiveX on the graphics page and then configure it in the runtime.

Was this helpful?
What can we do to improve the information ?