Technical FAQs

Ask a Question

We have to use web server, web clients with using Vijeo citect scada but web server local host port used by another application so, how can I assign another port for web client on VJC web server

For changing the localhost port 80 & 8080 we do not have any options,  but in general these ports can be accessed by many application at a time so it should work .
You can also set the port forwading settings in your router if you want to divert the request for the port 80 to some other port like 320. Then in internet browser you can try
using the other syntax for connecting the localhost Citect`s web page like "http://127.0.0.2/citect" or http://localhost:320/Citect. 
Was this helpful?
What can we do to improve the information ?