Technical FAQs

Ask a Question

Is it possible to adjust the bandwidth of Quantum NOE modules.

You can adjust the bandwidth between the NOE modules (140 NOE 771 01 and 140 NOE 771 11) and the CPU modules by configuring the number of messages
per cycle and the size of the messages in the configuration tab of the processor editor screen. This bandwidth improvement is effective when using Unity Pro under
TCP/IP for addressing the CPU in server mode (i.e., from an OFS tool).




Please note :
This functionality is only supported on CPU modules with version 2.80 or greater and NOE modules with version 4.60 or greater. 
                         Increasing this bandwidth has an impact on the cycle time of the processor.
Was this helpful?
What can we do to improve the information ?