Technical FAQs

Ask a Question

What is the replacement for the 490NRP95400 Fiber Optic Repeater.

The 140NRP95400 is the replacement for the 490NRP95400.This product is fully compatible with the legacy 490NRP95400.
All the existing topology's currently using the 490NRP95400 are supported by the 140NRP95400, including the one with redundant
cabling and / or optical loops for a maximum of network availability. In addition, you can mix both of them in the same network architecture.

In the worst case, when there is no available slot in the Quantum backplane, the customer will have to buy (1) 140NRP95400, (1) backplane, (1) PS
and to plug existing cables on the new NRP. In the best case, the customer will have to plug the 140NRP in the Quantum rack and just to re-connect the network.

Was this helpful?
What can we do to improve the information ?