Technical FAQs

Ask a Question

Does Modicon Quantum platform support IEC60870-5-104 protocol.

Yes, Quantum platform support IEC60870-5-104 protocol. PTQ-104C, IEC-60870-5-104 Client and  PTQ-104S IEC-60870-5-104 server are the modules
designed to be used on IEC60870-5-104 protocol.
These modules are created, designed and supplied by ProSoft Technology. These can be used in Quantum HSBY systems as well.
It is installed on Quantum local rack.
Was this helpful?
What can we do to improve the information ?