Technical FAQs

Ask a Question

How can I configure PTQ104 modules in unity pro.

In the local quantum rack add new device & expand the Communication tree, then select GEN NOM. This module type provides extended communication capabilities
for the Quantum system, and allows communication between the PLC and the PTQ module without requiring additional programming. Next enter the module personality
value, the correct value for this modules is 1060 decimal (0424 hex).
Was this helpful?
What can we do to improve the information ?