Technical FAQs

Ask a Question

Does the ATV212 drive come with conformal coating standard?

Issue:
Does the ATV212 drive come with conformal coating?

Product Line:
ATV212

Environment:
All

Cause:
Application requirement.

Resolution:
ATV212 is Conformal coated per  IEC 60721-3-3 classes 3C1 and 3S2 (chemical gases & solid particles ).
Was this helpful?
What can we do to improve the information ?