Technical FAQs

Ask a Question

How do I compare drive configurations files with SoMove Lite?

Customer wants to compare configurations between two drives 

Product Line:
ATV12, ATV312, ATV61, ATV71

All models and serial numbers


To compare configurations between two drives using SoMove Lite both drives have to be the same model number and both configuration files should be saved. 
1. Open one of the configurations,
2. Select "Compare Configurations" from the File menu,
3. Select the configuration file of the device you want to compare.
Both configuration files will be displayed on the screen.  The values highlighted are those parameters that are different.
Was this helpful?
What can we do to improve the information ?