Technical FAQs

Ask a Question

What is the part number for Simple Loader?

Issue:
What is the part number for Simple Loader to use with the Altivar 12, 312, 32, 61 and 71 drives?

Product Line:
Altivar 12, 312, 32, 61, 71, ATV12, ATV312, ATV32, ATV61, ATV71

Environment:
All catalog numbers

Cause:
Need to copy and transfer the same program between multiple drives.

Resolution:
Part number for the Simple Loader is VW3A8120.

The Instruction Bulletin is document number 30072-452-46. 
Was this helpful?
What can we do to improve the information ?