Technical FAQs

Ask a Question

What is the speed accuracy of the Altivar 12 drive.

Speed accuracy of the Altivar 12 drive is 2%  (accuracy between no load condition and nominal load).

Example:

For a 1440 rpm motor, speed will not change more than 28 RPM between loaded and no loaded condition.
Was this helpful?
What can we do to improve the information ?