Technical FAQs

Ask a Question

What is the m aximum operating altitude for Altivar 212 drive.

Maximum operating altitude for Altivar 212 drive is 1000 meter  without derating.
 
And for 1000…3000 meter : current derating of 1% per additional 100 meter.
 
Was this helpful?
What can we do to improve the information ?