Technical FAQs

Ask a Question

What is shock resistance and vibration resistance data for Altivar 32 drive.

Vibration resistance for Altivar 32:
1.5mm peak to peak (f=3...13Hz) conforming to EN/IEC 60068-2-6
1gn (f=13...200Hz) conforming to EN/IEC 60068-2-6
 
Shock resistance:
15gn for 11ms conforming to EN/IEC 60068-2-27
 
Was this helpful?
What can we do to improve the information ?