Technical FAQs

Ask a Question

what is the maximum number of Event logging entries possible in Event log in Vijeo Designer.

The maximum number of event logging entries available in Vijeo Designer is 10000.

But the default value is set for the entries of event loggig entries is 100 you can increase the value by going into the property of event logging
setting and change the value of total number of record.
Was this helpful?
What can we do to improve the information ?