Technical FAQs

Ask a Question

What is the relationship between register 3205 and what is displayed for OTR ( motor torque ) in menu 1.2 monitoring? How do I convert to % to match the display?

Issue: 
What is the relationship between register 3205 and what is displayed for OTR ( motor torque ) in menu 1.2 monitoring?

Product Line: 
Altivar 61 / 71 ATV61 ATV71

Environment:  
All

Cause:  
None

Resolution:  
3205 register stores the value of the motor torque as :
(C / Cn) * 1000
C : Motor torque (This parameter is the result of other characteristics).
Cn : Nominal motor torque

In the 1.2 MONITORING menu, OTR displays 3205 register value divided by 10. In that case, OTR displays the torque motor in % of the nominal torque (100% = Nominal torque). The scale is not depending of the drive HP rating because of the value is in % of the nominal torque.
Was this helpful?
What can we do to improve the information ?