Technical FAQs

Ask a Question

How to get the ATV61/71 to do a ramp stop when being controlled via communication bus?

Issue:
How to get the ATV61/71 to do a ramp stop when being controlled via communication bus?

Product Line:
ATV61 ATV71

Environment:
All

Cause:
When the stop command is removed, via communication, the VFD will free wheel stop?

Resolution:
There are 2 ways to resolve the issue:

1.       From the network Address 8652 (Parameter DOTD) should equal to 1
OR
2.       From the keypad Dis. Operate opt. Code should be set to Ramp
a.       Drive menu press enter
b.      Application function menu press enter
c.       Stop Configuration press enter
d.      Dis. Operate opt. Code set to ramp press enter
Was this helpful?
What can we do to improve the information ?