Technical FAQs

Ask a Question

How do you clear the SAFF status on the ATV32 drives?

How do you clear the SAFF status on the ATV32 drives?
Product Line:
Altivar ATV32
SAFF mode has been activated by opening one of the 3 safety inputs STO, SLS or SS1.
A: STO status on drive means the drive safety inputs STO, SLS or SS1 were assigned but not turned on during power up.
Power down the drive 1st leaving safety inputs turned OFF
With the drive powered down turn on any assigned safety inputs STO, SLS or SS1.
Power up the drive with the safety inputs turned on and it will show RDY.
B: SAFF status on the drive means after the drive was powered up in RDY  or is running and someone opened one of the safety STO, SLS, SS1 safety inputs.
To clear the SAFF power down the drive and make sure any assigned safety inputs are turned on or jumper to +24vdc before you power the drive back up. (For Testing purpose only).
Other things to check that can trigger a SAFF
Make sure Debounce time and response time are set to 0 for both to disable this function. Again if the values are out of range it can trigger a SAFF status.
Safety programming can only be done using SoMove programming software.

ATV32- password for STO is 1581
Was this helpful?
What can we do to improve the information ?