Technical FAQs

Ask a Question

How do you order a Masterpact NW or NT circuit breaker?


Issue:
What is the process for ordering a Masterpact NW or NT circuit breaker?

Product Line:
Masterpact NW and NT

Cause:
Masterpact breakers cannot be ordered by catalog number.

Resolution:
Masterpact circuit breakers cannot be ordered by catalog number.  A Schneider distributor or sales office must enter the order via the online product selector in My Schneider or Quote to Cash.
Information they need includes the certification standard (UL, ANSI, IEC), fixed or drawout, ampacity, AIR required, trip unit functions or type, accessories, connectors, and any other requirements.

The attached decoder will assist in breaking down a catalog number to its component parts.  With knowledge of the breaker's construction it will be possible to use the Q2C or E-way product selector to select, quote, and order the breaker.

Required information for placing an order can be found on the attached RFQ (Request for Quote).
Was this helpful?
What can we do to improve the information ?