Technical FAQs

Ask a Question

Can the ATS48 soft starter be started from the remote keypad?

Issue:
Can the ATS48 soft starter be started from the remote keypad?

Product Line:
ATS48 series SoftStarter

Environment:
All ATS48 series starters, all serial numbers

Cause:
Programming information not found in the programming manual

Resolution:
It is not possible to start the ATS48 series soft starter from the default or remote keypad.   Start/stop can be performed using the STOP/RUN terminals on the starter with either 2 wire or 3 wire configuration, or via Modbus RTU control.
Was this helpful?
What can we do to improve the information ?